STORY Mining

mtu Africa gives mining trucks a new lease on life

Posted on May 08, 2019, Images by mtu

Eight Komatsu and Hitachi trucks in Africa are currently being converted to mtu Series 4000 engines.
Solwezi, Sambia

mtu Africa, a subsidiary of Rolls-Royce Power Systems, has already successfully retrofitted multiple mining trucks with mtu engines and has recently added another eight projects to the list, converting three Komatsu 960-2KT and five Hitachi EH3500-AC2 mining vehicles. These were first-time retrofits on both types of vehicle. Last December and March of this year, staff from South Africa and Zambia worked on First Quantum Minerals’ Sentinel Mine in Zambia to repower the first  of three 960-2KT Komatsu trucks. In the rebuild, a competitor engine that had reached the end of its service life was replaced by a new 20-cylinder Series 4000 engine. The third project is to follow in May. The results of the first project once again confirm the classic virtues of mtu products: “all truck operators at the mine now prefer to drive the repowered truck”, which boasts outstandingly fast response characteristics at lower engine revolutions per minute. Other quintessential mtu strengths now gained by the repowering project are greater reliability and robustness, longer maintenance intervals and lower fuel consumption. The truck fleet used at the Sentinel mine includes not only the Komatsu trucks but eight Liebherr T284 mining trucks, also powered by mtu’s 20-cylinder  Series 4000 units, and two LeTourneau front-end loaders. mtu Africa has excellent credentials in mine-truck repowering, especially on Komatsu vehicles, and has in the past retrofitted Komatsu 730E, 860E-1K and 930E-4 trucks with mtu Series 4000 engines. 

Repowering of a 960-2KT mining truck with a 20-cylinder Series 4000 engine. Each project confirms the outstanding strengths of this series, in particular in terms of excellent fuel consumption, performance, reliability and uptime, long maintenance cycles and customer service quality – all superb customer benefits.

mtu Africa personnel were furthermore engaged by operator First Quantum in Zambia at its  Kansanshi mine to replace the competitors engine of a Hitachi EH3500-AC2 mining truck with a mtu 12-cylinder Series 4000. The Kansanshi mine is the largest copper mine in Africa, and five trucks in total are to be repowered there over the next few months. The tried-and-trusted mtu 12-cylinder Series 4000 is already powering two of the Hitachi EH3500-AC3 trucks at the same mine.  

Over 800 Series 4000 retrofits worldwide
It is always a compliment to mtu engines when they are retrofitted to mining trucks – especially when they replace other manufacturers' engines. Since the launch of the Series 2000 and Series 4000, they have been fitted to over 800 mine trucks as well as excavators, front-end loaders and surface blast hole drilling rigs worldwide, with the Series 4000 accounting for the lion's share. Each project confirms the outstanding strengths of this series, in particular in terms of excellent fuel consumption, performance, reliability and uptime, long maintenance cycles and customer service quality – all superb customer benefits.  The engines used are always bang-up-to-date versions. One major driver of lower total cost of ownership is the excellent fuel consumption. “As consumption accounts for around 80 to 85% of TCO, this is a key purchasing criterion for many customers,” emphasized Robert Wagner, Senior Manager Mining /Oil & Gas in Europe, the Middle East, Africa and Russia. 

Since the launch of the Series 2000 and Series 4000, they have been fitted to over 800 mine trucks as well as excavators, front-end loaders and surface blast hole drilling rigs worldwide, with the Series 4000 accounting for the lion's share. Last December and March of this year, mtu Africa staff repowered 960-2KT Komatsu trucks.

Mine trucks usually need new engines after three to five years. Rolls-Royce Power Systems supplies what it calls Repower Kits for this purpose. These are pre-assembled drive modules consisting of an engine, a generator and a radiator all mounted on a base frame. They also come with an electronic engine management and monitoring system. mtu engineers are happy and skilled to the task to  tailor-made technical adjustments where necessary. 

Across the world, the most potential for repowering with the Series 4000 can be found in Russia, the US, Australia, Chile, Peru, Africa and China. As one of the latest developments in Europe, the company is currently opening up markets in Bulgaria and Serbia.

The content of the stories reflects the status as of the respective date of publication. They are not updated. Further developments are therefore not taken into account.

Point of contact

Robert Wagner
Phone:
07541 90 4849
+49 7541 90 4849
+49 75417 90 4849
+49(0)7541 904849
Fax:
+49(0)7541 90904849
E-mail:

Related stories

Mining

Another 10,000 hours

With preventive maintenance, precise analysis of operating data and modern mtu engines, MTW engineers extend the service life of Komatsu 830E haul trucks while reducing operating costs.

Read more

Mining

Brazilian Mining and Construction Company Repowers Fleet with mtu Engines from Rolls-Royce

Rolls-Royce will deliver 30 Series 4000 mtu engines to U&M Mineração e Construção S/A, a leading earthworks contractor in Brazil.

Read more

Mining

mtu engines power machines at Modikwa Platinum Mine on South Africa’s rich mineral reef

Underground mining demands extreme performance for extreme periods, both for miner and machine. In a 24/7 operation, durability and efficiency are the building blocks to profitability. At Modikwa Platinum Mine, one of South Africa’s leading platinum mines, you will find some machines which perform Herculean feats in places that they have very little right to be in. Up to 800m underground in the mine, drill rigs and load haul dumpers powered by mtu Series 900 engines, add significantly to Modikwa’s profitability through their performance, durability and efficiency. In terms of performance it means minimal downtime, fuel efficiency and low emissions.

Read more