Um den Austoß von Stickoxiden zu reduzieren, wird ein Teil des Abgases gekühlt und der Ladeluft wieder beigemischt.
STORY

How does Exhaust Gas Recirculation work?

Posted on June 17, 2014, Images by mtu

To reduce nitrogen oxide emissions, a proportion of the exhaust gases is cooled and then reintroduced into the charge-air.
Friedrichshafen, Gernany

Nitrogen oxide (NOX) emissions can be reduced using internal engine technology by cooling some of the exhaust gas, which is then redirected back into the charge air. This results in the reduction of the combustion temperature and less nitrogen oxide is produced. This process is known as exhaust gas recirculation (EGR) and is one of the principal methods used to reduce nitrogen oxide emissions from diesel engines. mtu has been developing this important technology and the functions and components associated with it since the beginning of the 1990s. It was first introduced in series production in mid-2011 for Series 4000 Oil and Gas engines in hydro-fracking applications (EPA Tier 4 emissions standard). It was likewise introduced in rail engines subject to EU IIIB emissions regulations which came into force in 2012.

Ways to reduce nitrogen oxide emissions


One of mtu´s aims for its engines is to reduce theemission of soot particles and nitrogen oxides in order to achieve compliance with increasingly strict emissions regulations around the world. The main approach pursued by mtu is low-emission combustion, in other words an internal engine solution. However, this means taking into account a basic principle that governs the process of combustion — if the fuel burns at a higher temperature inside the cylinder, little soot is produced, but a large amount of nitrogen oxide. At lower combustion temperatures, nitrogen oxide emissions are low, but the production of soot particulates is high. To find the right balance, therefore, all the key technologies that affect combustion must be perfectly matched. When combined with fuel injection and turbocharging in particular, the use of exhaust gas recirculation results in a combustion process that produces significantly lower levels of nitrogen oxide. The second way of reducing nitrogen oxide emissions is to use exhaust gas aftertreatment with an SCR catalytic converter (selective catalytic reduction, short: SCR). Very low limits for both nitrogen oxide and diesel particulates can make the use of such an SCR system necessary. Exhaust gas recirculation
can reduce nitrogen oxide emissions by around 40 percent. Depending on the application, SCR systems remove up to 90 percent of the nitrogen oxide from exhaust gases. In the case of particularly stringent emission standards, exhaust gas recirculation and a SCR system must be combined to ensure the limits are met.
Fig. 1: Integration of exhaust gas recirculation in engine design concept mtu has integrated the exhaust gas recirculation system into the engine design so that it has very little effect on space requirements.

Examples of EGR use in mtu drive systems


For mobile applications in excess of 560 kW, US EPA Tier 4 interim emissions regulations which have been in force since 2011 stipulate maximum emissions of 3.5 g/kWh. This applies to mtu Series 1600, 2000 and 4000 engines. Series 2000 and 4000 units meet the targets using exhaust recirculation technology. Series 1600, 2000 and 4000 locomotive engines subject to European EU Stage IIIB emissions rules in force since 2012 are also equipped with EGR systems. Nitrogen oxide and hydrocarbon (HC) emissions combined may not exceed 4.0 g/kWh. By contrast, the limit for NOX emissions for railcars in the same EU Stage IIIB emission standard is only 2.0 g/kWh. For this reason, mtu is equipping its Series 1600 engines for under floor drive systems with an SCR exhaust aftertreatment — with no exhaust gas recirculation. The US EPA Tier 4 final regulations which came into force for mobile machines below 560 kW in 2014 are particularly stringent. In this case, the nitrogen oxide limits are down 90 percent to 0.4 g/kWh compared with EPA Tier 3 regulations. To meet these demanding targets, mtu uses both exhaust recirculation technology and an SCR system. As the introduction of Tier 4 final emissions regulations involves no further tightening of NOX values, mtu will retain ist exhaust gas recirculation technology. mtu´s aim is to use in-engine technology to achieve compliance with the stricter particulate limits. This will involve optimization and further development of the injection and combustion systems and of turbocharging technology.
Fig. 2: Schematic diagram of exhaust gas recirculation In exhaust gas recirculation, some of the exhaust gas is returned to the fresh air intake. The resultant mixture of fresh air and exhaust gas has a lower calorific value in terms of the volume. This lowers combustion chamber temperatures, thus reducing the production of nitrogen oxide (NOX).

Benefits of exhaust gas recirculation from mtu


Generally speaking, systems designed to reduce emissions must be modified to match the drive systems. mtu has produced a very compact design that permits all the exhaust gas recirculation components to be integrated into the engine concept (see Figure 1), so that any modifications to the engine have relatively little effect on space requirements and the exhaust system. It is necessary to modify the radiator, however, in order to cope with the increased cooling capacity of the engine. Compared to engine modifications involving an SCR system, this makes it much easier for customers to convert their units to meet new emissions standards because EGR systems for reducing nitrogen oxides require no additional operating media and thus involve no further expense or work on extra tanks and lines. The customer
benefits in terms of reduced costs for handling and maintenance.

Principle of operation


In exhaust gas recirculation, some of the exhaust gas is drawn off from the exhaust system, cooled and redirected back into the cylinders (see Figure 2). Although the exhaust fills the combustion chamber, it is not involved in the combustion reaction that takes place in the cylinder due to its low oxygen content. The speed of the combustion
process overall is thus reduced, with the result that the peak flame temperature in the
combustion chamber is lowered. This dramatically reduces the production of nitrogen oxides.

Patented solution from mtu: the donor cylinder concept


Exhaust gas recirculation places higher demands on exhaust gas turbocharging, since
higher boost pressures have to be achieved with reduced mass flow in the turbocharging system. These high boost pressures are required to direct
the increased mass flow resulting from the exhaust gas recirculation rate into the cylinder during the gas cycle. In addition, the exhaust gas can only be redirected back into the cylinders when there is a pressure drop between the exhaust and the charge air systems. This pressure drop must be established with an appropriately configured turbo charging system, which results in a reduction in turbocharging efficiency. The pressure drop between the exhaust and the charge air systems leads to gas cycle los - ses. These factors tend to result in lower engine performance or higher fuel consumption. To improve the combined effect of exhaust gas recirculation and turbocharging, mtu has developed what is known as the donor cylinder exhaust gas recirculation system (see Figure 3). mtu’s patented system only uses some of the engine’s cylinders as the donor for exhaust gas recirculation. An exhaust valve (donor valve) holds back the exhaust gas flow downstream of the donor cylinders and thus creates the necessary pressure drop between the exhaust and the charge air systems. This means that the turbocharging system can be optimized to a very good efficiency level, with gas cycle losses only affecting the donor cylinders. Compared with conventional high-pressure exhaust gas recirculation (as in the case of the Series 1600 engine), the donor cylinder concept (Series 2000 and 4000) achieves lower fuel consumption, since it reduces the gas cycle losses in the engine and permits higher turbocharger efficiency levels. For this purpose, an additional donor cylinder exhaust valve is required in comparison with high-pressure exhaust gas recirculation. Dirt build-up on components and the amount of servicing required over the service life of the application are lower with the donor cylinder concept, as is the case with high-pressure exhaust gas recirculation: unlike the situation with low-pressure exhaust gas recirculation, the exhaust gas is not fed into the intake air until immediately
before it enters the cylinder, which means that only clean air flows through the
compressor impeller and the intercooler and not exhaust gas containing particles as well.
Fig. 3: EGR donor cylinder concept Compared with conventional high-pressure exhaust gas recirculation, mtu’s patented system achieves lower fuel consumption, since it reduces the gas cycle losses in the engine and permits higher turbocharger efficiency levels. This requires an additional donor cylinder exhaust valve.

Cooling system for exhaust gas recirculation


The exhaust gas drawn off for recirculation has a temperature of around 650 degrees Celsius. It is therefore far too hot to be fed directly into the cylinders; it would increase the temperature of the combustion chamber even further, thereby defeating its actual purpose — that of reducing nitrogen oxide formation by lowering the combustion temperature. For this reason, the exhaust gas is first cooled to around 120 degrees Celsius (see Figure 4). In the case of industrial engines with high intake air and exhaust mass flow rates that requires high cooling capacities, which have to be supplied by high-performance heat exchangers. In principle, proven volume-production coolers as used in the commercial vehicle sector can be adopted for the purpose. However, to cover the cooling capacity required for a 16-cylinder engine with a capacity of 4.8 liters per cylinder, depending on the supplier, four to eight conventional commercial vehicle radiators of the highest capacity available would be needed for exhaust gas recirculation. Using this number of single radiators with the required mechanical strength is not possible in a mobile application. mtu is therefore working with its suppliers to develop integrated cooler solutions in which only the internal components of the heat exchangers from proven commercial vehicle applications are adopted and the highly integrated cast housing is developed specifically to match individual requirements. The heat exchanger body is designed to match the contours of the engine perfectly and incorporates all connecting pipes. The benefits for the customer are a smaller space requirement, high functional reliability and low maintenance. mtu uses as many common parts as possible for engines within the same series with different numbers of cylinders. Due to the advanced
stage of development maturity, this also results in a high level of functional reliability.
Fig. 4: Section through a radiator The exhaust gas drawn off for recirculation at a temperature of around 650 degrees Celsius is far too hot to be fed directly into the cylinders. For this reason, the exhaust gas is first cooled to around 120 degrees Celsius. The cooling system is optimally integrated into the engine design concept, so that the customer needs only to allow for a very small space requirement.

Interaction with other key technologies


Although exhaust recirculation results in lower nitrogen oxide emissions, soot particulate emissions increase to an undesirable degree if no counter-measures are taken. To prevent this happening, mtu has further refined both fuel injection and
turbocharging. Whether a diesel particulate filter (DPF) is needed in addition to these internal engine modifications to further reduce emissions depends on the limits specified in the emission standard applicable to the individual application.

Summary


Exhaust gas recirculation is one of mtu’s key internal engine technologies for reducing emissions. It can be used to reduce nitrogen oxide formation inside the cylinder by 40 percent and more, with the result that many applications — depending on the applicable limits in each case — can meet the required emission stan dards without the need for additional exhaustaftertreatment for NOX removal. In cases where emissions legislation is particularly strict, an SCR system or even a combination of exhaust gas recirculation and SCR system is required. mtu has produced a compact solution to integrate all the exhaust gas recirculation components into the engine design concept so that no additional installation space is required (see Figure 5). It means that customers can upgrade their applications to comply with new emission standards with no great effort involved. The system also requires no additional consumables.
Fig. 5: Comparison of 16V 4000 R43 engine for rail applications with no EGR and 16V 4000 RX4 with EGR mtu first introduced exhaust gas recirculation in series production in mid-2011 for Series 4000 Oil and Gas engines in hydro-fracking applications (EPA Tier 4 emissions standard). It was likewise introduced in rail engines subject to EU IIIB emissions regulations which came into force in 2012. As the individual components are efficiently integrated on the engine, virtually no additional space is required (see illustrated comparison with Series 4000 rail engine without exhaust gas recirculation).


Point of contact

Dr Johannes Kech
Phone:
+49 7541 90 2153
E-mail:

Related stories

How does Common Rail Injection work?

Common rail injection allows the combustion process to be optimized so that less pollutant is produced from a smaller amount of fuel.

Read more

How does a Diesel Particulate Filter work?

Diesel particulate filters can be used to remove most of the soot particles from diesel engine exhaust gases.

Read more

How does Selective Catalytic Reduction work?

Selective catalytic reduction employs chemical reduction to render nitrogen oxides harmless.

Read more

Turbocharging: Key technology for high-performance engines

Turbochargers give engines their power and their unmistakable character.

Read more