MTU zeigt neben einem historischen Motor das aktuelle Portfolio an Bahnmotoren.
STORY Rail

A view of the mtu booth

Posted on September 24, 2014, Images by Ralf Rühmeier

mtu showcases an engine from bygone days, and next to it, its current rail portfolio.
Berlin, Germany

Never was an mtu engine so celebrated by the public. In May 1933, the 'Hamburger Flyer' high-speed diesel train, powered by the GO-5, entered Hamburg main station to rapturous applause. It had just completed the Berlin-Hamburg line in less than 21/2 hours - at the time, a sensation. Karl Maybach's achievement was not just development of the GO-5 engine with 410 HP. Besides equipment in the immediate periphery of the engine such as the mountings, the air and fuel supply lines, the exhaust pipework and the engine cooling system, he had also developed the vehicle cooling system and the transmission.

The content of the stories reflects the status as of the respective date of publication. They are not updated. Further developments are therefore not taken into account.

Point of contact

Rolf Behrens Spokesman Trade Media Mobile Power Solutions
Phone:
+49 7541 90 3461
E-mail:

Related stories

Rail

"We could already be saving 90% of CO₂ today – but we prefer to discuss it."

A conversation with Dr. Olaf Toedter (Head of New Technologies and Ignition Systems at the Karlsruhe Institute of Technology) and Jörg Schneider (Head of Sustainability at DB Cargo) about HVO, eFuels, and the technologies that no one can see yet.

Read more

Rail

Cruise Train on rails

Superlative in every respect, the Train Suite Shiki-Shima is powered by electricity generated by two mtu Series 4000 engines on non-electrified routes.

Read more

Rail

Special Purpose Railway Vehicles

Read more