Rolls-Royce has commissioned ten mtu gas gensets in northern Egypt to supply the Egyptian Wood Technology Company's (WOTECH) production plant with electricity. Since there is no access to the public grid, Wotech relies entirely on the mtu gensets. The factory produces medium-density fibreboard (MDF) from rice straw, which is used for furniture and buildings. The plant avoids the usual practice of burning rice straw, which is a by-product of rice cultivation, and ensures its sustainable use. Rolls-Royce hat im Norden Ägyptens zehn mtu-Gasaggregate in Betrieb genommen, die die Produktionsanlage der Egyptian Wood Technology Company (WOTECH) mit elektrischer Energie versorgen. Da es keinen Zugang zum öffentlichen Stromnetz gibt, verlässt sich Wotech vollständig auf die mtu-Aggregate. In der Fabrik produziert das Unternehmen mitteldichte Faserplatten (MDF) aus Reisstroh, die für Möbel und Gebäude verwendet werden. Die Fabrik vermeidet die übliche Praxis, Reisstroh, das als Nebenprodukt beim Reisanbau anfällt, zu verbrennen, und sorgt für eine nachhaltige Nutzung.
PRESS RELEASE Power Generation

mtu gas gensets from Rolls-Royce supply electricity for Africa’s first rice straw MDF production facility

Posted on January 08, 2025

Images [1 Files, 4 MB]

  • Egyptian Wood Technology Company (WOTECH) relies entirely on mtu island solution for energy supply
  • Factory is the second of its kind in the world and the first in Africa, and reduces air pollution and CO2 emissions

Rolls-Royce has commissioned ten mtu gas gensets in the Beheira province in northern Egypt to supply the Egyptian Wood Technology Company's (WOTECH) production plant with electricity. Since there is no access to the public grid, WOTECH relies entirely on the 20-cylinder mtu gas gensets, which together have a total output of 25 megawatts.

The factory produces medium-density fibreboard (MDF) from rice straw, which is used for furniture and buildings. Supported by Egypt's petroleum ministry, the plant avoids the usual practice of burning rice straw, which is a by-product of rice cultivation, and ensures its sustainable use by repurposing it into MDF. The factory is the second of its kind in the world and the first in Africa. It significantly reduces air pollution and CO2 emissions in Egypt. The rice straw replaces traditional wood as a raw material in medium-density fibreboard, which is used to make cabinets, doors, furniture and commercial and residential buildings.

Rolls-Royce worked with local partner Engineering for Industries Co. (INDE) and the Egyptian Maintenance Company (EMC), a provider of engineering support services in the region, to supply the mtu Series 4000 L64 FNER gensets, controls and accessories for the WOTECH project, which was established with full Egyptian capital from the oil sector.

Tobias Ostermaier, President Stationary Power Solutions at Rolls-Royce, said: “When supporting a project such as the WOTECH facility, where there is no access to the grid utility, the dependability of our mtu gas-powered gensets is paramount. Working with INDE and EMC, we were able to deliver a power solution that met all the customer requirements - being efficient, reliable and offering the combination of best-in-class power density with low emissions.”

Each of the 10 mtu gensets has a rated power of 2,500 kW and an operational lifetime of up to 84,000 hours before needing major overhaul (TBO).

About Rolls-Royce Holdings plc

  1. Rolls-Royce is a force for progress; powering, protecting and connecting people everywhere. Our products and service packages help our customers meet the growing need for power across multiple industries; enable governments to equip their armed forces with the power required to protect their citizens; and connect people, societies, cultures and economies together.
  2. Rolls-Royce has a local presence in 47 countries and customers in over a hundred more, including airlines and aircraft leasing companies, armed forces and navies, and marine and industrial customers.
  3. Through our multi-year transformation programme, we are building a high-performing, competitive, resilient and growing Rolls-Royce. We are building the financial capacity and agility to allow us to successfully develop and deliver the products that will support our customers through the energy transition.
  4. Annual underlying revenue was £20.1 billion in 2025, and underlying operating profit was £3.46 billion.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
  6. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,350 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.

www.rolls-royce.com

Contact

Jennifer Riley Spokeswoman North and Latin America
Phone:
+1 248 560 8488
E-mail: