PRESS RELEASE Power Generation

Avacon and Rolls-Royce are testing the contribution of battery storage and PV systems to grid stability

Posted on April 15, 2025

  • Field tests are investigating the intelligent integration of renewable energies with home storage systems and larger mtu battery storage systems
  • Objective: to contribute to the efficient energy supply of energy communities and grid support

German energy supplier Avacon and Rolls-Royce together are driving forward the integration of battery storage into the power grid as part of a research project. Based on a field test, the aim is to show how energy communities, PV systems and mtu battery storage can be intelligently linked to contribute to an efficient energy supply and to stabilize the energy system. Avacon and Rolls-Royce are already collaborating on a second research project. The aim is to use battery storage to moderate generation peaks from PV systems and bring them into line with electricity consumption.

Lower Saxony's Minister for Economic Affairs, Olaf Lies (SPD), symbolically commissioned the mtu battery storage system in northern Germany, together with Avacon's Chief Technology Officer Rainer Schmittdiel and Lukas Köhler, Managing Director Sales and Service Germany at Rolls-Royce Power Systems.

Speaking at the commissioning ceremony, Lukas Köhler of Rolls-Royce Power Systems said: “We are delighted to be working with Avacon again. The intelligent linking of our mtu battery storage system with PV systems and home storage systems, which is to be tested in the project, makes an important contribution to both the energy transition and grid stabilization. Battery solutions are among our strategic business areas and ensure energy security worldwide.”

Intelligent linking of storage systems and renewable energies relieves power grid
The project is based on the concept of an energy community: local households store electricity they generate themselves from PV systems in home storage units, and surplus energy is also fed into the central mtu large-scale battery storage system. The interaction between home and large-scale battery storage is controlled by means of intelligent algorithms. On the one hand, this should help to balance out the volatility of power generation from PV systems. On the other hand, the project aims to increase the local self-consumption rate to up to 100 percent at times. This relieves the power grid and increases the overall stability of the system.

mtu battery solutions from Rolls-Royce ensure energy security worldwide
Rolls-Royce supplies large-scale battery solutions that consist of modular units for capacity and power and can be flexibly configured to any size. The components include integrated battery cabinets and the mtu EnergetIQ intelligent control system. They are used primarily for grid services, energy trading and the integration of renewable energies. The mtu EnergetIQ control platform ensures optimal performance and flexibility.

About Rolls-Royce Holdings plc

  1. Rolls-Royce is a force for progress; powering, protecting and connecting people everywhere. Our products and service packages help our customers meet the growing need for power across multiple industries; enable governments to equip their armed forces with the power required to protect their citizens; and connect people, societies, cultures and economies together.
  2. Rolls-Royce has a local presence in 47 countries and customers in over a hundred more, including airlines and aircraft leasing companies, armed forces and navies, and marine and industrial customers.
  3. Through our multi-year transformation programme, we are building a high-performing, competitive, resilient and growing Rolls-Royce. We are building the financial capacity and agility to allow us to successfully develop and deliver the products that will support our customers through the energy transition.
  4. Annual underlying revenue was £20.1 billion in 2025, and underlying operating profit was £3.46 billion.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
  6. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,350 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.

www.rolls-royce.com

Contact

Silke Rockenstein Spokeswoman Trade Media
Phone:
+49 7541 90 7740
E-mail: