PRESS RELEASE Power Generation

Rolls-Royce supplies mtu emergency power systems for the European Commission

Posted on March 12, 2025

Images [3 Files, 4 MB]

  • Emergency power systems based on 20-cylinder Series 4000 mtu engines secure new Jean Monnet 2 building complex in Luxembourg
  • mtu gensets guarantee the operation of all safety-related equipment within seconds in the event of a power outage

Rolls-Royce has won the order to supply two mtu Series 4000 generator sets to provide emergency backup power for the European Commission in Luxembourg. The two gensets, each with a maximum output of 2,640 kVA, were installed by Rolls-Royce partner Energolux in the new Jean Monnet 2 building complex at the beginning of October as part of the renovation and expansion of the Commission.

Jean Monnet 2 is designed to bring together several currently dispersed offices of the European Commission. The planned complex will consist of a welcome pavilion, a tower over 20 floors high, and a lower, flat-roofed building. The buildings provide space for approximately 3,700 employees and include modern office space, conference rooms, an auditorium, restaurants, fitness and health centres, and logistics areas.

The mtu gensets will provide reliable emergency power for the Jean Monnet 2 building complex. They ensure that all essential and safety-related equipment inside the buildings, as well as their technical systems, can continue to operate without interruption in the event of a power outage.

The mtu emergency backup gensets, model 20V4000 DS2750, are high-performance diesel generators specifically designed to provide electrical power in the event of a grid outage. “The emergency backup gensets are characterized by their high reliability and efficiency,” said Alain Osuch, Directeur Commercial Travaux Neufs at Energolux. “This makes them the ideal solution for such critical applications.”

With the delivery of the mtu emergency gensets, Rolls-Royce is making an important contribution to the completion of the EU’s construction project, which is expected to be finalized in 2025.

“We are proud that our mtu emergency gensets will help ensure the operational reliability of the European Commssion,” said Vittorio Pierangeli, Vice President Global Powergen at Rolls-Royce's Power Systems division. “This is further proof of the trust our customers place in the quality and reliability of our products and is fully in line with our strategy of providing products to secure critical infrastructure.”

Rolls-Royce protects critical infrastructure worldwide
Rolls-Royce offers mtu emergency power solutions based on diesel and gas generators as well as dynamic UPS systems that are used to protect critical infrastructure. Worldwide, more than 85,000 mtu emergency power systems secure data centers, industrial facilities, airports, hospitals, power plants and numerous other types of buildings that require an uninterruptible power supply.

About Rolls-Royce Holdings plc

  1. Rolls-Royce is a force for progress; powering, protecting and connecting people everywhere. Our products and service packages help our customers meet the growing need for power across multiple industries; enable governments to equip their armed forces with the power required to protect their citizens; and connect people, societies, cultures and economies together.
  2. Rolls-Royce has a local presence in 47 countries and customers in over a hundred more, including airlines and aircraft leasing companies, armed forces and navies, and marine and industrial customers.
  3. Through our multi-year transformation programme, we are building a high-performing, competitive, resilient and growing Rolls-Royce. We are building the financial capacity and agility to allow us to successfully develop and deliver the products that will support our customers through the energy transition.
  4. Annual underlying revenue was £20.1 billion in 2025, and underlying operating profit was £3.46 billion.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
  6. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,350 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.

www.rolls-royce.com

Contact

Silke Rockenstein Spokeswoman Trade Media
Phone:
+49 7541 90 7740
E-mail: