Die Twitter User von ScotRail haben für einen pinken Bahn-Motor gestimmt.
STORY Rail

Pretty in Pink

Posted on September 06, 2019, Images by Abellio ScotRail

ScottRail's Twitter users voted for a pink engine
Edinburgh, United Kingdom

mtu rail engines are usually spray-painted blue or red. Since 28 August 2019, ScotRail has been able to boast a pink-finished mtu 16V 4000 unit in its Inter7City 43127 locomotive. The Scottish train operator decided to hold a vote among Twitter followers on the color of the engine, giving them a choice of yellow, turquoise or pink. Over 2,000 took part, with the color pink carrying the day. 

The engine had been sent to MTU UK in East Grinstead for QL3 maintenance, which takes place halfway through the service life (TBO). A face-lift in the form of a new spray of paint is part of the service package, and ScotRail decided on a new pink look for one of its rail engines, which are usually grey. “It was Alan Stewart, ScotRail's service delivery manager for HSTs, who phoned to tell us about the campaign,” grinned Rod Riley, mtu Service Manager. “Maybe we will suddenly find a big demand for pink engines,” added sales colleague David Eaton. 

ScotRail is introducing 26 fully upgraded InterCity high-speed trains for its services between Scotland’s seven cities. Each train has two locomotives, each powered by a 16V 4000 unit. From now on, that means a fleet of 53 grey engines, with one painted pink. The trains are in service in Scotland, connecting the cities of Aberdeen, Dundee, Edinburgh, Glasgow, Inverness, Perth and Stirling. 

The content of the stories reflects the status as of the respective date of publication. They are not updated. Further developments are therefore not taken into account.

Point of contact

David Eaton
Phone:
+44 (0) 1342 335 481
+44 1342 335 481
E-mail:

Related stories

Rail

"We could already be saving 90% of CO₂ today – but we prefer to discuss it."

A conversation with Dr. Olaf Toedter (Head of New Technologies and Ignition Systems at the Karlsruhe Institute of Technology) and Jörg Schneider (Head of Sustainability at DB Cargo) about HVO, eFuels, and the technologies that no one can see yet.

Read more

Rail

Cruise Train on rails

Superlative in every respect, the Train Suite Shiki-Shima is powered by electricity generated by two mtu Series 4000 engines on non-electrified routes.

Read more

Rail

Special Purpose Railway Vehicles

Read more